Missing Symbol Definitions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Missing Symbol Definitions

3,091 Views
fixed-term_juli
Contributor I

I use the 3-Phase PMSM Motor Control Development Kit with Qorivva MPC5604P MCU and the User interface of NXP you can see ins Screen.PNG.

If I start the program, there is a failure -Missing symbol Definitions- you can see at Variables.PNG.

But it is connected with the board. (Communication.PNG)

Where is the problem and how can I fix it?

(The motor runs if I use the switch up/down or I update the target with the User interface. But there is no change if I vary the input variables)

0 Kudos
Reply
1 Reply

3,005 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

Did you follow quick start guide and compiled and loaded the code to micro?

Do you have correctly set Freemaster files?

regards,
Peter

0 Kudos
Reply