Maximum MPC5644A eTPU2 frequency

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Maximum MPC5644A eTPU2 frequency

Jump to solution
3,027 Views
EAlepins
Contributor V

Hi,

 

Neither the datasheet nor the reference manual of MPC5644A states what is the maximum allowed frequency for the eTPU2. The eTPU2 can run at system clock, ok, but is it allowed to put the system clock at 150MHz when the eTPU is enabled and configured at fsys? Indeed, other devices of MPC56xx family usually limit the eTPU around 132MHz...

 

Thanks.

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
2,755 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

In general eTPU2 can run at 200MHz at most.

eTPU on MPC5644A can run at 150MHz when configured for full system clock. Note that eTPU graphical configuration tool use maximum value 145MHz, but qualified device is capable to achieve 150MHz. It is needed to edit c:\Program Files (x86)\Freescale\eTPU Graphical Configuration Tool\conf\etpucpu.ini and fix max system clock for MPC5644A to 150MHz:

[MPC5644A]

module=eTPU2

engines=1

system_clock=150

etpu_clk_prescaler=1

STAC_bus_available=Yes

template=template_MPC5644A

View solution in original post

0 Kudos
Reply
3 Replies
2,756 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

In general eTPU2 can run at 200MHz at most.

eTPU on MPC5644A can run at 150MHz when configured for full system clock. Note that eTPU graphical configuration tool use maximum value 145MHz, but qualified device is capable to achieve 150MHz. It is needed to edit c:\Program Files (x86)\Freescale\eTPU Graphical Configuration Tool\conf\etpucpu.ini and fix max system clock for MPC5644A to 150MHz:

[MPC5644A]

module=eTPU2

engines=1

system_clock=150

etpu_clk_prescaler=1

STAC_bus_available=Yes

template=template_MPC5644A

0 Kudos
Reply
2,755 Views
EAlepins
Contributor V

Thanks. Again, can this be added to documentation please?

0 Kudos
Reply
2,755 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I don't see the reason for that. MCU's system clock cannot run above 200MHz. Currently there is no device running above 200MHz excluding 264MHz with MPC5674F in Enhanced mode (IPCLKDIV = 0) where however fetpu=fsys/2.

In my eyes it would be redundant information.

0 Kudos
Reply