MPC57XX Uart Send Problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC57XX Uart Send Problem

2,649 次查看
mikailaltintas
Contributor III

Hi, I have problem about uart send functionality.  If there is no data on receive I can send data but if data received when I send data  ,the program will stop at 

                                                       while (LINFlexD_0.UARTSR.B.DTFTFF == 0);

I put a secureCounter to while loop so it is go on working but I want to know why this happens. If I increase baud rate I see that event occurrence decrease. So I think that uart is not work full dublex.  Manual Reference says Uart is Full duplex but it is working as half dublex. 

My configuration is listed below:

 

nbLINFlex = 0;

LINFLEX[nbLINFlex]->LINCR1.B.INIT = 1; // enter initialization mode


LINFLEX[nbLINFlex]->UARTCR.B.UART = 1; //0=LIN 1=UART
LINFLEX[nbLINFlex]->UARTCR.B.PCE = 0; //0 = parity disabled, 1 = parity enabled
LINFLEX[nbLINFlex]->UARTCR.B.PC0 = 0; //0 = even parity, 1 = odd parity
LINFLEX[nbLINFlex]->UARTCR.B.WL0 = 1; //0 7-bit data + parity bit *** 1 8-bit data (or 9-bit if PCE is set).

LINFLEX[nbLINFlex]->UARTCR.B.TxEn = 1;
LINFLEX[nbLINFlex]->UARTCR.B.RxEn = 1;


LINFLEX_InitRxBuffer(nbLINFlex,1);

LINFLEX[nbLINFlex]->UARTSR.B.DRFRFE = 1; // clear DRF flag (Data Reception Complete Flag)
LINFLEX[nbLINFlex]->UARTSR.B.DTFTFF = 1; // clear DTF flag (Data Transmission Complete Flag)
LINFLEX[nbLINFlex]->LINCR1.B.INIT = 0; // enter normal mode

 

Is there any solution to solve this. 

标签 (1)
标记 (3)
2 回复数

2,525 次查看
mikailaltintas
Contributor III

Hi,

I found solution. Problem is about clearing DRFRFE flag.

In ISR I use  

LINFLEX[0]->UARTSR.B.DRFRFE = 1;

to clear flag. When I use this also DTFTFF flag clearing. So 

while (LINFlexD_0.UARTSR.B.DTFTFF == 0); is locked.

We have to use 

LINFlexD_0.UARTSR.R &= 0x00000004;

to clear DRFRFE flag. 

0 项奖励
回复

2,525 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

yes, this is common issue when bit access is used; read-modify-write instruction is executed and so other flags can be cleared too.

See more info in chapter 3.2 of https://www.nxp.com/docs/en/engineering-bulletin/EB758.pdf

BR, Petr