MPC5777c Programming UTEST Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5777c Programming UTEST Problem

1,687件の閲覧回数
marv_marsian
Contributor II

Hello,

I have used the instructions listed in Solved: MPC5777C update DCF record - NXP Community to program STCU2 module. I made a mistake and wrote a wrong value in my xxx.srec file, thus to the 0x00400310 address. I tried to overwrite it but the PROGPPCNEXUS program throws `Error during programming` error(nothing else).

I already read that UTEST flash area cannot be deleted, but is it also non-re-writable? Is there a way to over-write this address?

Thanks to anyone who reads. 

Best wishes. 

0 件の賞賛
返信
1 返信

1,673件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Ekrem,

I'm afraid there's no solution for this. Erase is not allowed and cumulative programming is also not allowed - only one program operation is allowed per 64-bit ECC segment.

If you made a mistake in UTEST, the only option is usually to replace the chip.

Regards,

Lukas