MPC5777c Programming UTEST Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5777c Programming UTEST Problem

1,674 Views
marv_marsian
Contributor II

Hello,

I have used the instructions listed in Solved: MPC5777C update DCF record - NXP Community to program STCU2 module. I made a mistake and wrote a wrong value in my xxx.srec file, thus to the 0x00400310 address. I tried to overwrite it but the PROGPPCNEXUS program throws `Error during programming` error(nothing else).

I already read that UTEST flash area cannot be deleted, but is it also non-re-writable? Is there a way to over-write this address?

Thanks to anyone who reads. 

Best wishes. 

0 Kudos
Reply
1 Reply

1,660 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Ekrem,

I'm afraid there's no solution for this. Erase is not allowed and cumulative programming is also not allowed - only one program operation is allowed per 64-bit ECC segment.

If you made a mistake in UTEST, the only option is usually to replace the chip.

Regards,

Lukas