MPC5777M UART+DMA problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5777M UART+DMA problem

1,640件の閲覧回数
underdangerous
Contributor II

Hi,community:

When I configure LINFlexD in UART mode and use it with DMA, for UART TX mode, data can be transmitted normally, but for UART RX mode, data in UART FIFO (LINFLEXD. BRDM) cannot be transmitted to RAM normally through DMA. I configure the corresponding TCD and peripheral DMA request sources according to Tables 7-25 and 7-26 in MPC5777MRM, but UART RX DMA seems to have not been executed correctly, which has been bothering me for a long time, I hope you can help me, thank you very much!The attachment contains the corresponding source code and values in the registers.

タグ(3)
0 件の賞賛
返信
1 返信

1,625件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

With receive LinFlex DMA channel, you have set CITER/BITER to zero. I don't think it would be correct.

davidtosenovjan_0-1690466682972.png

 

タグ(1)
0 件の賞賛
返信