MPC5777C bootloader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5777C bootloader

Jump to solution
3,909 Views
1620773328
Contributor II

I am using s32ds . I wanted start with boot loader for MPC5777C.

Situation1:We want to  update firmware (one on one) for device though CAN1, BRT=1Mbps, because the CAN0 already used for CANFD. 

Situation2:We want to to update firmware for specified device through CAN bus that a lot of devices hanging on it.

Is there application note and any reference code . Thanks!

Best Regards

Jinus

 

0 Kudos
Reply
1 Solution
3,905 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

we have this application note:

https://www.nxp.com/docs/en/application-note/AN5319.pdf

https://www.nxp.com/docs/en/application-note-software/AN5319SW.zip

It's serial bootloader for MPC5748G microcontroller but I believe it could be a nice start point for you.

Regards,

Lukas

 

View solution in original post

0 Kudos
Reply
2 Replies
3,906 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

we have this application note:

https://www.nxp.com/docs/en/application-note/AN5319.pdf

https://www.nxp.com/docs/en/application-note-software/AN5319SW.zip

It's serial bootloader for MPC5748G microcontroller but I believe it could be a nice start point for you.

Regards,

Lukas

 

0 Kudos
Reply
3,846 Views
1620773328
Contributor II

Hi Lukas,

Can you share with me the source code project (S32_PA) for mpc5777c can bootloader ? I wanna do some advanced development based on your project. Thanks very much.

Regards .

Jinus

0 Kudos
Reply