MPC5777C Memory Protection Unit (MPU) 2 Cores

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5777C Memory Protection Unit (MPU) 2 Cores

ソリューションへジャンプ
2,571件の閲覧回数
MPC_Mike
Contributor I

I'm developing the MPC5777C to run multicore. 2 Cores one using HW I/O(Core1), one without using HW I/O(Core0). I want to use the MPU to protect memory regions. 

Is this possible?

How can this be done?

0 件の賞賛
返信
1 解決策
2,560件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

yes, it is possible. Configuration of the MPU is relatively simple and it depends on your requirements. We have this SW example written for MPC5674F:

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5674F-MPU-Initialization-CW210/ta-p/1...

MPU on MPC5674F is almost the same as on MPC5777C. Just check the differences in Word 2 of the descriptor because there are different bus masters.

Regards,

Lukas

 

元の投稿で解決策を見る

3 返答(返信)
2,558件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

To avoid confusion, I will add that there are two instances of MPU module on MPC5777C to cover all the resources. So, it is necessary to initialize both modules.

lukaszadrapa_0-1614156745474.png

 

 

0 件の賞賛
返信
2,561件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

yes, it is possible. Configuration of the MPU is relatively simple and it depends on your requirements. We have this SW example written for MPC5674F:

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5674F-MPU-Initialization-CW210/ta-p/1...

MPU on MPC5674F is almost the same as on MPC5777C. Just check the differences in Word 2 of the descriptor because there are different bus masters.

Regards,

Lukas

 

2,525件の閲覧回数
MPC_Mike
Contributor I

thanks! we havent exhaustively gone through this but it seems to be what we're looking for

0 件の賞賛
返信