In the S32DS, how to see the DEMO of the running light is built in the form of SDK,
is there any example that does not use the form of SDK to build direct modification
Hi,
which SDK demo do you refer to?
Within S32DS you can find several examples that are not based on SDK.
BR, Petr
Where can I find a DEMO of it
My real opinion is not SDK based
How to configure the input and output parameters of a GPIO
Hi,
pin is configured using SIU.MSCRn register. See RM for more info and IO signal table attached to the RM.
to have pin working as GPIO keep SIU.MSCRn[SSS] cleared and for
- output set SIU.MSCRn[OBE] and control output level using SIU.GPDOn
- input set SIU.MSCRn[IBE] and read input level from SIU.GPDIn
BR, Petr