MPC5748G uSDHC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5748G uSDHC

2,499件の閲覧回数
yang104hong
Contributor II

Hello! Is there any examples or documents where I can find information on how to configure and use uSDHC on MPC5748G?

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,254件の閲覧回数
jimledin
Contributor I

Hello Lukas,

Would it be possible to provide a short example that will help get us started with uSDHC on MPC5748G? I'm interested in the SD 4-bit I/O mode. I would like to see how to configure the uSDHC and set up the pins (it's not clear to me how the pins that are both input and output should be configured) and then send commands to and receive responses from the card. Thank you!

-- Jim

0 件の賞賛
返信

2,254件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hello Jim,

I have asked around if there are plans to provide drivers for uSDHC. I will let you know later...

Regards,

Lukas

0 件の賞賛
返信

2,254件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

currently there are no SW examples for uSDHC. The only description of the module can be found in the reference manual.

Regards,

Lukas

0 件の賞賛
返信