MPC5748G uSDHC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5748G uSDHC

2,497 Views
yang104hong
Contributor II

Hello! Is there any examples or documents where I can find information on how to configure and use uSDHC on MPC5748G?

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

2,252 Views
jimledin
Contributor I

Hello Lukas,

Would it be possible to provide a short example that will help get us started with uSDHC on MPC5748G? I'm interested in the SD 4-bit I/O mode. I would like to see how to configure the uSDHC and set up the pins (it's not clear to me how the pins that are both input and output should be configured) and then send commands to and receive responses from the card. Thank you!

-- Jim

0 Kudos
Reply

2,252 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hello Jim,

I have asked around if there are plans to provide drivers for uSDHC. I will let you know later...

Regards,

Lukas

0 Kudos
Reply

2,252 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

currently there are no SW examples for uSDHC. The only description of the module can be found in the reference manual.

Regards,

Lukas

0 Kudos
Reply