MPC5748G RAM Memory Map Question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5748G RAM Memory Map Question

ソリューションへジャンプ
2,006件の閲覧回数
kmh48301
Contributor IV

Hello

I have question in MPC5748G RM Page129

and I need to solve this question for my task..

kmh48301_1-1614908983472.png

 

1. What does the STANDBY mean?

2. According to that table, RAM memory has 6 Section. Why are they separate?

3. I guess that Section1 is for RAM Vector Table and Section 2 is for customSectionBlock 

  But I have no idea about Section3-6.

(I refered the linker flash.ld file)

Is my guess correct? I need to make it sure.

 

Any help please

 

Thanks

Best Regards

Phillip

0 件の賞賛
返信
1 解決策
1,996件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Standy RAM is part of RAM which remains powered in low power modes. So you can use it for operation with minimum consumption.

RAM is not divided for any purpose. You can use it as you want.

best regards,

Peter

元の投稿で解決策を見る

1 返信
1,997件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Standy RAM is part of RAM which remains powered in low power modes. So you can use it for operation with minimum consumption.

RAM is not divided for any purpose. You can use it as you want.

best regards,

Peter