MPC5748G ESW setup problems

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5748G ESW setup problems

2,533 Views
Daniel_Wax
NXP Employee
NXP Employee

My customer is having issues setting up the ESW such that all traffic coming into port 0 will be forwarded to port 1.  They just need this to be pass through.

I started looking at the switch stack 

SW5748G-ETHSS1-BETA-0.9.0

but I think that will just confuse the matter.

Do we have any example of this very simple setup

@markusregner   Markus does the register setup you just posted have all traffic forwarding?  Maybe I could start there

 

 

 

 

0 Kudos
Reply
3 Replies

2,526 Views
markusregner
NXP Employee
NXP Employee

I'm not sure and the setup I posted is faulty itself, hence unreliable. However if you start from 0 you may want to pick up Technica-Engineering's configuration because at least something seems to work.

0 Kudos
Reply

2,519 Views
Daniel_Wax
NXP Employee
NXP Employee

Thanks Markus.  I don't see this in the community.  Is this something they sell?

 

BTW do you know if there are header files for MPC5748G with ESW support?  Our Beta example switch stack seems to use Macros.  

 

@Crisno_Yi_Yang   Yi Can you help with this one?

0 Kudos
Reply

2,487 Views
Crisno_Yi_Yang
NXP Employee
NXP Employee
Hello, Daniel I have no example which could be directly run, I noticed that we have provided two stack for this case:SWITCH_STACK_MPC574XX and FAST_PATH_ROUTER_MPC574XX_EAR_0.8.0. And I have sent the head file supported ESW by email. BR Yi
0 Kudos
Reply