MPC5746 Internal TVS current level

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5746 Internal TVS current level

Jump to solution
3,692 Views
RheaGao
Contributor I

Hi,

 I am using SPC5746R chip to design the minimum system with 1.25V using the following same circuit. During the debugging process, I found that 5746 would not work if I did not add Clv 1uF buffer capacitor to write the program with 200M main frequency. Specifically, I was stuck in the clock initialization and could not pass.  What mechanism triggers the microcontroller to cause this?  Thanks!

 

 

0 Kudos
Reply
1 Solution
3,672 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Rhea,

 

Do you mean that 1uF capacitor is the only one at VDD_LV? The specification says that minumum capacitance is 4.7uF:

lukaszadrapa_0-1651474177761.png

And it’s minimal value. It should be validated by user for given application.

It is also recommended to use Progressive Clock Switching feature to avoid current spikes. Search for „Progressive Clock Switching“ in the reference manual for details.

Regards,

Lukas

View solution in original post

0 Kudos
Reply
1 Reply
3,673 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Rhea,

 

Do you mean that 1uF capacitor is the only one at VDD_LV? The specification says that minumum capacitance is 4.7uF:

lukaszadrapa_0-1651474177761.png

And it’s minimal value. It should be validated by user for given application.

It is also recommended to use Progressive Clock Switching feature to avoid current spikes. Search for „Progressive Clock Switching“ in the reference manual for details.

Regards,

Lukas

0 Kudos
Reply