MPC5744P debugger stucked

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5744P debugger stucked

3,610件の閲覧回数
renhaochen
Contributor II

Dear all:

I met some problem when using MULTILINK UNIVERSAL FX to debug our own product which is use MPC5744P as the controller, and it was in S32DS.

When I start debugging, the progress shows 98%, and the console stops with the message below:

"

CMD>VC

Verifying object file CRC-16 to device ranges ...

   block 00FA0000-00FA0007 ...

"

But with the sample project and source code, this situation doesn't happened in DEVKIT.

Is anybody had met this kind of problem and knows how to fix it?

Thank you.

タグ(2)
4 返答(返信)

3,247件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

it seems your issue is the same as in the thread below.

https://community.nxp.com/thread/473662 

Please check this thread and eventually send me back the same information. It seems this is about incorrect debugger settings.

Regards,

Martin

2,620件の閲覧回数
lzheng
Contributor II

I met exactly the same problem. Replacing with another control board resolved the issue. Therefore, it is not related to the debug setting or firmware issue. 

I need to find out the root cause as this is for production. Any solutions or explanation why it failed? 

0 件の賞賛
返信

3,247件の閲覧回数
yanronglu
Contributor II

Hi Martin:

            I had this problem, too, where the power off while I was programming, and then I had this problem.Can the chip be reused?

0 件の賞賛
返信

3,247件の閲覧回数
renhaochen
Contributor II

Hi Martin:

 

Thank you for replying, but the situation is not as same as that thread

Why cannot programming the mpc5744P? 

Instead, I solved this problem by changing a new MPC5744P micro controller.

I assume that maybe the old one is not functionally OK.

0 件の賞賛
返信