SPC5643L question summary

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPC5643L question summary

1,658件の閲覧回数
yulong
Contributor II

Hi NXP team,

I have some question about SPC5643L

I use CW 10.6,Matlab 2015a, use MBD but not NXP MBDT

At present, my operation efficiency is much lower than the previous scheme, so I have several questions to confirm

1.I need to use single precision floating-point, is my setting optimal? Do you need to set up floating point libraries elsewhere

My setting:C/C++ Build ->Settings-> Floating Point->SPFP_Only

2.Do you have a CW version of the PWM triggered AD DMA collection routine

3.I use Matlab 2015a, Can I use NXP MBDT? Is this a free tool? Is there a version of SPC5643L for my version?

 

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,591件の閲覧回数
yulong
Contributor II

Thanks 

That solved some of my problems

0 件の賞賛
返信

1,642件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

1.I need to use single precision floating-point, is my setting optimal? Do you need to set up floating point libraries elsewhere

My setting:C/C++ Build ->Settings-> Floating Point->SPFP_Only

See following thread:

https://community.nxp.com/t5/CodeWarrior-Development-Tools/enable-floating-point/m-p/462312

2.Do you have a CW version of the PWM triggered AD DMA collection routine

If you are asking about example code. Then I do not find any for such scenario.

3.I use Matlab 2015a, Can I use NXP MBDT? Is this a free tool? Is there a version of SPC5643L for my version?

I dont think you can use it with v 2015a. But you can have a look at release notes of MDBT.

In case you wont find information in release note, please rise a question on MDBT forum, they could give you the most accurate answer.

https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/bd-p/mbdt

Yes, it is free of charge.

 

petervlna_0-1698045263701.png

Best regards,

Peter

 

 

 

0 件の賞賛
返信