[MPC5744P]FCCU+SWT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[MPC5744P]FCCU+SWT

933 Views
Sxhdjw
Contributor I

Dear NXP officers:

  Hi, i got  trouble with the FCCU_mpc5744p example u offered in S32DS . 

 1. when i program the chip and  press SW1 , the alarm led begins shining for period time since FCCU fault has worked and system switch to alarm status. when i try to  press SW2 to clean fault, the alarm led turn off in a moment.  But when i release the SW2, the alarm led shine again.so why?

here's some details :I change SW1 ,SW2 and alarm led  because I didn't use the official core board. by the way , i also change the SIUL_ISR channel to 243 in intc_SW_mode_isr_vectors_MPC5744P.c. before this step , if i didn't change the channel ,the led even didn't work.
 2. I also try to use the software watch dog for my project. According to the short reset example from the forum . it  truly works to reset but it didn't back to _start from the reset . Besides i cant watch any info from the debugger cauese the core is offline.

0 Kudos
Reply
2 Replies

922 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I have looked at the main.c you have provided. It looks like majority  of FCCU setting is copied from mine codes.

Unfortunately author of the example, is no longer in NXP so I can't ask him about the example.

Whole example seems to me awkward.

However I can guide you quite easy trough the process.

Write me what you really want to do with FCCU and I can guide you.

Also I have written some applicaiton notes along with examples SW for MPC5744P FCCU.

You can start by reading them and looking into examples to understand how FCCU works first:

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MPC574xP-FCCU-configuration-guide/ta-p/1105448

Best regards,

Peter

0 Kudos
Reply

899 Views
Sxhdjw
Contributor I

Hi,

Thanks for reply, I actually want to do the software watchdog function(SWT) . Besides, I have referenced the sample code "Example MPC5744P SWT Short reset GHS614". And in fact its really works on my mpc5744p device .But, as what i say in the last inquire,  the SWT works but it didn't go into  _start and the cpu hanged up , i cant read any info from the s32 debugger. so i guess if there is any problem in FCCU after reset because it didn't go from the SAFE status to NORMAL status . To verify my guess , i try to use ur FCCU example to prove it . That's all . Is there any advice offer for me? I truly need the SWT in my project.

0 Kudos
Reply