MPC5744P DMA bus error to get data from source

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5744P DMA bus error to get data from source

1,662 Views
edwardlu666
Contributor II

Hello:

Now I debug the DMA module of MPC5744P.BUT BUS ...

DMA reading occurs the bus error.And FAE from Shanghai-Office tells me it would not be the permitted to access the bus for DMA.  (Why source bus error?)

here is my debug sight from LAUTERBACH

ES.jpg

All AIPS opened for no-supervisor mode:

AIPS.jpg

Could any one help me?

thanks 

2 Replies

1,474 Views
edwardlu666
Contributor II

question resolved by setting AIPS and SMPU register to make the ram accessable.the code should be in start up,but in my project,transform the code in the later stage... not reasonable but can work

thanks all 

1,474 Views
edwardlu666
Contributor II

Buffer is located in the RAM so does this matters?or can some of the register to be set to correct the error?

0 Kudos
Reply