MPC5744 Datasheet Error About Pin D[12]

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5744 Datasheet Error About Pin D[12]

2,901件の閲覧回数
cagataykaleliog
Contributor I

Hello,

 

There is an error in the datasheet of MPC5744P. It is marked with a red box in the attached section of the datasheet.

 

It is not clear which SPI module's (DSPI 1 or DSPI3) SOUT output can be connected to pin D[12].

There are alternative SOUT pins for both of these modules but I hope that this issue leads to an overall check of all SPI module pins.

 

Regards,

 

Cagatay

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,728件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hi,

this reference manual typo is already reported. It should be fixed in addendum, which will be released next month.

Correct function is DSPI3 SOUT.

Regards,

Martin

0 件の賞賛
返信

2,728件の閲覧回数
cagataykaleliog
Contributor I

Thank you.

Regards,

Cagatay

0 件の賞賛
返信