MPC5744 Datasheet Error About Pin D[12]

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5744 Datasheet Error About Pin D[12]

1,105 Views
cagataykaleliog
Contributor I

Hello,

 

There is an error in the datasheet of MPC5744P. It is marked with a red box in the attached section of the datasheet.

 

It is not clear which SPI module's (DSPI 1 or DSPI3) SOUT output can be connected to pin D[12].

There are alternative SOUT pins for both of these modules but I hope that this issue leads to an overall check of all SPI module pins.

 

Regards,

 

Cagatay

Labels (1)
0 Kudos
Reply
2 Replies

932 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

this reference manual typo is already reported. It should be fixed in addendum, which will be released next month.

Correct function is DSPI3 SOUT.

Regards,

Martin

0 Kudos
Reply

932 Views
cagataykaleliog
Contributor I

Thank you.

Regards,

Cagatay

0 Kudos
Reply