MPC5744 Datasheet Error About Pin D[12]

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5744 Datasheet Error About Pin D[12]

2,929 次查看
cagataykaleliog
Contributor I

Hello,

 

There is an error in the datasheet of MPC5744P. It is marked with a red box in the attached section of the datasheet.

 

It is not clear which SPI module's (DSPI 1 or DSPI3) SOUT output can be connected to pin D[12].

There are alternative SOUT pins for both of these modules but I hope that this issue leads to an overall check of all SPI module pins.

 

Regards,

 

Cagatay

标签 (1)
0 项奖励
回复
2 回复数

2,756 次查看
martin_kovar
NXP Employee
NXP Employee

Hi,

this reference manual typo is already reported. It should be fixed in addendum, which will be released next month.

Correct function is DSPI3 SOUT.

Regards,

Martin

0 项奖励
回复

2,756 次查看
cagataykaleliog
Contributor I

Thank you.

Regards,

Cagatay

0 项奖励
回复