MPC5743

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5743

3,129 Views
xuan
Contributor I

HI,

Can MPC5743 implement IO interrupt?

Can you send me a project example?

0 Kudos
Reply
6 Replies

3,122 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Yes, it can do interrupt via IO.

Please refer to reference manual chapter 16.3.4.1 External interrupt initialization.

Futhermore the available examples are in S32DS:

petervlna_0-1697618985302.png

and also here:

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MPC5-software-example-list/ta-p/1102445#MPC5744P

Best regards,

Peter

 

0 Kudos
Reply

3,107 Views
xuan
Contributor I

HI,

Can you get back to me as soon as possible? Thank you very much

0 Kudos
Reply

3,119 Views
xuan
Contributor I

HI

Thank you very much for your reply

Can you give me a specific link to which example project it is?

0 Kudos
Reply

3,097 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I do not know if there is a direct example for what you looking for. I have not find it.

However you can use this one instead as a guide:

https://community.nxp.com/docs/DOC-343728

The devices are very familiar, same SIUL2, same INTC.

Best regards,

Peter

0 Kudos
Reply

3,093 Views
xuan
Contributor I
HI,
Thank you very much,
The routines in the link are very helpful to me, but the routines in the link are based on MPC5748, what I need is MPC5743 routines, can you help me find one based on MPC5743
0 Kudos
Reply

3,087 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

As I have said. I didn't find one directly for SPC5744P.

But you can use the SPC5748G as template. They use the same IP modules.

With little porting, it should work with no issues.

Best regards,

Peter

0 Kudos
Reply