MPC5675K and parallel GPIO Pad Data In Register

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5675K and parallel GPIO Pad Data In Register

1,816 Views
CorderBollie
Contributor II

Hello

 

We have an application running in decoupled parallel mode (DPM) on a MPC5675K.

A Samsung K9F1G08 Flash is connected via GPIOs where GPIO[0]..[7] are connected to I/O0..7 of the flash module.

 

If we read a huge amount of data from the flash device we get a lot of ECC errors and sometimes at least one byte is completely wrong.

While reading the data we use a gpio to toggle RE line of the flash device and read in the data via the parallel GPIO Pad Data In Register 0 (SIUL.PGPDI[0]).

 

We tried to read PGPDI[0] twice and the errors are gone like:

 

void psp_nand_gpio_read ( uint8_t * dest, uint32_t length )

{

  RE_HI;

  WE_HI;

  while ( length-- )

  {

    RE_LO;

    /* Wait some time. */

    wait_nand( PULSE_WIDTH );

    /* Read data. */

    *dest = ( *(volatile uint8_t *)( SIUL_BASE + 0x0C40u ) );

    *dest++ = ( *(volatile uint8_t *)( SIUL_BASE + 0x0C40u ) );

    RE_HI;

  }

} /* psp_nand_gpio_read */

 

If we do that we are able to read all bytes without error. If we read only once we will get errors.

 

The question is what can cause that behaviour?

Labels (1)
0 Kudos
Reply
1 Reply

1,520 Views
PetrS
NXP TechSupport
NXP TechSupport

hi,

Seems there could be timing issue  when accessing the external memory. Unless that code is interrupted or other core accesses/modifies “dest” area. If the latter one is not a case, check if there is always enough time between RE assertion and data read (to follow memory specification) and also the time between RE  negation and assertion again.

Have you checked the reading with the scope or some analyzer? Try to compare the values in buffer for  single reading and for repeated one (use 2 buffers here, do not write to single one). Is the result somehow comparable?


Regards,

Petr

0 Kudos
Reply