qadc in continuous mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

qadc in continuous mode

2,962 次查看
izzetozcelik
Contributor I

I am trying to use QADC attached to DMA in continuous mode. I can use in them in Software Single Scan  by trigerring the QADC in software.

When I set the QADC mode to continuous scan software mode, even it is armed by the EDAM it does not start executing the commands meaning that

it does not get triggerred.

 

How do you trigger the QADC in continuous scan software mode?

 

note: I use  MPC5554 and MPc56644a.

 

Best regards

izzet

标签 (1)
0 项奖励
回复
2 回复数

2,811 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

CFIFO starts automatically after being configured into this mode (Continuous Scan Software Triggered).

I would recommend to use other CFIFO (for instance CFIFO1) for initial ADC configuration, trigger it by single scan, wait for EOQ flag and then use CFIFO that is being used with continuous mode (for instance CFIFO0). Conversion starts automatically.

0 项奖励
回复

2,812 次查看
izzetozcelik
Contributor I

Thanks for the reponse. I managed to get it running. I was initially set it to single scan then to continuou scan. I think the first single scan setting was blocking the QADC to move into continuous scan mode.

It seems working.

I confirm by understanding from your response too. Thanks.

I am planning to put the project for other people who donot have any experience with MPC5xxx.

regards

izzet

0 项奖励
回复