MPC5674F Unable to capture an external interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5674F Unable to capture an external interrupt

1,986 Views
volpato
Contributor I

I'm having trouble setting MPC5674F to capture an external interrupt. I tried to adapt the examples from AN2865 Qorivva Simple Cookbook and also tried to follow the steps dictated in MPC5674F Reference Manual, but without success.

My goal is to capture an interrupt via signal EMIOS14_IRQ0_GPIO193 using INTC in HW vector mode. (I also tried SW vector mode too, but couldn't make it work).

Could you please provide an example for this scenario?

Labels (1)
0 Kudos
Reply
1 Reply

1,511 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Try to see following example, it is the same principle:

Example MPC5606B SIUL External interrupt

0 Kudos
Reply