MPC5645S DCU3 Maximum Panel size.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC5645S DCU3 Maximum Panel size.

跳至解决方案
1,402 次查看
peteradamcik
Contributor III

HI Guys, we're going to be using the DCU3 in the MPC5645S and in the manual it says maximum TFT panel size is Wide VGA 800x480. Could the DCU3 run a 800x600 panel? The DCULite can have a panel up to 1024x768 but our 176PIN MPC5645S LQFP does not incorporate the DCULite, only the DCU3.

So do you think the DCU3 could drive an 800x600 RGB Panel?

Please let me know. 

Thanks guys

Pete

 

0 项奖励
回复
1 解答
1,381 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Probably not. DCU3 itself is capable to deliver resolution up to Wide VGA (800 x 480).

AN4865 described also impact of used memories - it mentions resolution up to 480 x 272 (WQVGA). I assume higher resolution had no sense to analyze.

davidtosenovjan_0-1631797083948.png

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,382 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Probably not. DCU3 itself is capable to deliver resolution up to Wide VGA (800 x 480).

AN4865 described also impact of used memories - it mentions resolution up to 480 x 272 (WQVGA). I assume higher resolution had no sense to analyze.

davidtosenovjan_0-1631797083948.png

 

0 项奖励
回复