MPC5645S DCU3 Maximum Panel size.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5645S DCU3 Maximum Panel size.

Jump to solution
1,395 Views
peteradamcik
Contributor III

HI Guys, we're going to be using the DCU3 in the MPC5645S and in the manual it says maximum TFT panel size is Wide VGA 800x480. Could the DCU3 run a 800x600 panel? The DCULite can have a panel up to 1024x768 but our 176PIN MPC5645S LQFP does not incorporate the DCULite, only the DCU3.

So do you think the DCU3 could drive an 800x600 RGB Panel?

Please let me know. 

Thanks guys

Pete

 

0 Kudos
Reply
1 Solution
1,374 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Probably not. DCU3 itself is capable to deliver resolution up to Wide VGA (800 x 480).

AN4865 described also impact of used memories - it mentions resolution up to 480 x 272 (WQVGA). I assume higher resolution had no sense to analyze.

davidtosenovjan_0-1631797083948.png

 

View solution in original post

0 Kudos
Reply
1 Reply
1,375 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Probably not. DCU3 itself is capable to deliver resolution up to Wide VGA (800 x 480).

AN4865 described also impact of used memories - it mentions resolution up to 480 x 272 (WQVGA). I assume higher resolution had no sense to analyze.

davidtosenovjan_0-1631797083948.png

 

0 Kudos
Reply