MPC5644B FLEXCAN module

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5644B FLEXCAN module

2,187件の閲覧回数
muhammadrafique
Contributor I


Hi All,

 

I have MPC5644B and i am using Flexcan 0 on it.The problem i am facing is that after transmitting first frame,Flexcan dosen't transmit any other frame. The CAN module is receiving frames just fine?

Thanks in advance for help.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,005件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I'm not sure what's wrong when reading this short description but I can provide very simple example that works as expected. It just sends data from CAN0 to CAN1 and everything is working as expected. See please attachment.

Regards,

Lukas

0 件の賞賛
返信

2,005件の閲覧回数
eunjolee
Contributor I

Thank you very much.

Eunjo Lee

0 件の賞賛
返信

2,005件の閲覧回数
gurumurthykola
Contributor I

Hi All,

I also faced the same issue in FlexCAN module of MPC5777C controller. It is transmitting only one CAN frame. after that the FlexCAN is put into Freeze Mode. It is happening with Receive also. After receive one frame the FlexCAN module is put into Freeze mode.

Please help anybody.

Thanks in advance.

Regards,

Gurumurthy K

0 件の賞賛
返信