MPC5644B FLEXCAN module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5644B FLEXCAN module

2,213 Views
muhammadrafique
Contributor I


Hi All,

 

I have MPC5644B and i am using Flexcan 0 on it.The problem i am facing is that after transmitting first frame,Flexcan dosen't transmit any other frame. The CAN module is receiving frames just fine?

Thanks in advance for help.

Labels (1)
0 Kudos
Reply
3 Replies

2,031 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I'm not sure what's wrong when reading this short description but I can provide very simple example that works as expected. It just sends data from CAN0 to CAN1 and everything is working as expected. See please attachment.

Regards,

Lukas

0 Kudos
Reply

2,031 Views
eunjolee
Contributor I

Thank you very much.

Eunjo Lee

0 Kudos
Reply

2,031 Views
gurumurthykola
Contributor I

Hi All,

I also faced the same issue in FlexCAN module of MPC5777C controller. It is transmitting only one CAN frame. after that the FlexCAN is put into Freeze Mode. It is happening with Receive also. After receive one frame the FlexCAN module is put into Freeze mode.

Please help anybody.

Thanks in advance.

Regards,

Gurumurthy K

0 Kudos
Reply