MPC5644A - eDMA Trial

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5644A - eDMA Trial

Jump to solution
2,535 Views
ShadowShooTR
Contributor III

Hi all,

I just want to transfer data from source to destination like ;

Source : uint8 g_uchSource[12]  --> the address is 0x40001e80

Source variables are : 0x00 , 0x11 , 0x22 , 0x33, 0x44 , 0x55, 0x66 , 0x77, 0x88, 0x99, 0xAA , 0xBB

Destination : uint16 g_untGhostHold[6].  --> the address is 0x40001e8c

The DMA TCD is arranged as :

EDMA.TCD[CH2].SADDR = (vuint32)&g_uchSource;
EDMA.TCD[CH2].DADDR = (vuint32)&g_untGhostHold;
EDMA.TCD[CH2].CITER = (vuint16)3;
EDMA.TCD[CH2].BITER = (vuint16)3;
EDMA.TCD[CH2].SSIZE = 0;  //8 bit source size
EDMA.TCD[CH2].DSIZE = 1;  //16 bit destination size 
EDMA.TCD[CH2].NBYTES = 4; //4 bytes will be transferred for each major iteration
EDMA.TCD[CH2].SLAST = (vuint32)(-1*12);  //return
EDMA.TCD[CH2].CITERE_LINK = 0;
EDMA.TCD[CH2].BITERE_LINK = 0;
EDMA.TCD[CH2].BWC = 0;
EDMA.TCD[CH2].DLAST_SGA = (vuint32)(-2*6); //return
EDMA.TCD[CH2].SMOD = 0;
EDMA.TCD[CH2].DMOD = 0;
EDMA.TCD[CH2].SOFF = 1; //Source minor address iteration will be 1 byte
EDMA.TCD[CH2].DOFF = 2; //Destination 2 byte
EDMA.TCD[CH2].MAJORE_LINK = 0;
EDMA.TCD[CH2].MAJORLINKCH = 0;
EDMA.TCD[CH2].E_SG = 0;
EDMA.TCD[CH2].D_REQ = 0;
EDMA.TCD[CH2].INT_HALF = 0;
EDMA.TCD[CH2].INT_MAJ = 0;
EDMA.TCD[CH2].ACTIVE = 0;
EDMA.TCD[CH2].DONE = 0;
EDMA.TCD[CH2].START = 0; 

Then I set the TCD.START bit in the software.

I expected that it would work like this :

1. Major (CITER = 3)

 -  1.Minor -> read(0x40001e80) , read(0x40001e81)

                      write(0x40001e8c)

 -  2.Minor -> read(0x40001e82) , read (0x40001e83)

                      write(0x40001e8e)

 2. Major (CITER = 2)

 -  1.Minor -> read(0x40001e84) , read(0x40001e85)

                     write(0x40001e90)

 - 2. Minor -> read(0x40001e86) , read(0x40001e87)

                     write(0x40001e92)

3. Major (CITER = 1)

 - 1. Minor -> read(0x40001e88), read(0x40001e89)

                      write(0x40001e94)

 - 2. Minor -> read(0x40001e8A), read(0x40001e8B)

                      write(0x40001e96)

Then Majors are complete, TCD.DONE will be set. 

However it didn't work as I expected.

 

In experiment : 

After the first major iteration ,DMA stops. CITER decreased just once and 4 byte transfer occured as shown below. 

ShadowShooTR_1-1613551446211.pngShadowShooTR_4-1613551773479.png

ShadowShooTR_5-1613552639714.png

Then I set the TCD_START bit manually.

ShadowShooTR_6-1613552760858.png

Then other 4 byte transferred correctly.  CITER decreased again.

ShadowShooTR_7-1613552841522.pngShadowShooTR_8-1613552866392.png

 

Again, I set TCD_Start bit manually , The TCD_DONE bit is set at this time.

ShadowShooTR_9-1613553003544.pngShadowShooTR_10-1613553054154.png

ShadowShooTR_11-1613553273925.png

 

All transfers were done correctly by setting  TCD_START bit manually for every major iteration break, but the question is that why doesn't DMA continue to work by itself after the first major iteration done until TCD_DONE occurs  ?

 

I searched referance manual (Page 589), it's given a similar example but it is hardware request. 

There is a sentence like this : 

ShadowShooTR_12-1613553491843.png

Probably , eDMA goes idle in my case right ? 

I do this transfer with single request just setting CITER = 1 and NBYTE = 12. It works.

I tried different channel but no change.

Do I have to do this transfer with hardware request ? But it's not any specific signal or module. 

Thank you in advance.

Best regards.

SS.

 

 

 

 

 

0 Kudos
Reply
1 Solution
2,516 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, it is correct behavior. Every time CITER is decreased, new DMA request is needed. DMA request means either HW request from other module or assertion of START bit by SW.

davidtosenovjan_0-1613560074347.png

 

View solution in original post

3 Replies
2,517 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, it is correct behavior. Every time CITER is decreased, new DMA request is needed. DMA request means either HW request from other module or assertion of START bit by SW.

davidtosenovjan_0-1613560074347.png

 

2,506 Views
ShadowShooTR
Contributor III

Hi,

I thought that those minor requests will trigger by themselves until major complete. That was the hardware request. I missed this point. Thank you so much @davidtosenovjan.

 

0 Kudos
Reply
2,415 Views
berat24
Contributor III

.

0 Kudos
Reply