MPC5644A Clock Frequency Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5644A Clock Frequency Problem

1,512件の閲覧回数
kadiraktas
Contributor III

Hi everyone,

I wanna ask a question. When I try to set frequency to 100 MHz (MPC5644A), I don't success. But if I try to set frequency up to 82 MHz, there is no problem.

I see some examples project which include following definitions  (" #define FLASH_REG FLASHA.BIUCR.R "and " #define FLASH_DATA 0x00018C55")

pastedImage_2.png

There is no information about these definitions on DataSheet for MPC5644A. Do you think this is real reason ? (When I add these definitons I can set high frequencies)

0 件の賞賛
返信
1 返信

1,431件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

this is already discussed here:

https://community.nxp.com/thread/507917 

Regards,

Lukas

0 件の賞賛
返信