MPC5644A Clock Frequency Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5644A Clock Frequency Problem

1,538 Views
kadiraktas
Contributor III

Hi everyone,

I wanna ask a question. When I try to set frequency to 100 MHz (MPC5644A), I don't success. But if I try to set frequency up to 82 MHz, there is no problem.

I see some examples project which include following definitions  (" #define FLASH_REG FLASHA.BIUCR.R "and " #define FLASH_DATA 0x00018C55")

pastedImage_2.png

There is no information about these definitions on DataSheet for MPC5644A. Do you think this is real reason ? (When I add these definitons I can set high frequencies)

0 Kudos
Reply
1 Reply

1,457 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

this is already discussed here:

https://community.nxp.com/thread/507917 

Regards,

Lukas

0 Kudos
Reply