MPC5634M  Flash_program   example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5634M  Flash_program   example

1,792 Views
sufree
Contributor II

Hi,

   I now learn to write a bottom drive of MPC5634M  Flash_program,but i face a lot of problem.so l need a exapmle to reference.The follow is what i have writed .

Who can give me a reference example ?

 

#ifdef ROM_VERSION
#pragma push
#pragma section code_type ".my_ram" ".my_ram" code_mode=far_abs
#endif
void Program_FLASH(void)
{
#define FLASH_HLR_PASSWORD 0xB2B22222
unsigned int status;
/* enable high address space */
CFLASH1.HLR.R = FLASH_HLR_PASSWORD; // unlock register
CFLASH1.HLR.R = 0x00000000; // unlock all high blocks

/* step1. erase block 10 (0xC0000-0xFFFFF) */
CFLASH1.MCR.B.ERS = 1; // select operation (erase)
CFLASH1.HSR.R = 0x00000004; // select 10 block
*((unsigned int*) p_test) = 0xFFFFFFFF; // interlock write
CFLASH1.MCR.B.EHV = 1; // start the erase operation
while(CFLASH1.MCR.B.DONE == 0){}; // wait for DONE
CFLASH1.MCR.B.EHV = 0;
CFLASH1.MCR.B.ERS = 0;

/* step2. program data */
CFLASH1.MCR.B.PGM = 1;
*((unsigned int*) p_test++) = data_to_be_written[0]; // first write
*((unsigned int*) p_test++) = data_to_be_written[1]; // additional write
*((unsigned int*) p_test++) = data_to_be_written[2]; // additional write
*((unsigned int*) p_test) = data_to_be_written[3]; // additional write
CFLASH1.MCR.B.EHV = 1; //start the erase operation
while(CFLASH1.MCR.B.DONE == 0){}; //wait for DONE
status=CFLASH1.MCR.R&0x00000200;
CFLASH1.MCR.B.EHV = 0;
CFLASH1.MCR.B.PGM = 0;
}

#ifdef ROM_VERSION
#pragma pop
endif

Labels (1)
0 Kudos
Reply
1 Reply

1,468 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

this piece of code works as expected:

  CFLASH1.HLR.R = 0xB2B22222; //password
  CFLASH1.HLR.R = 0x0; //unlock all blocks in high address space in CFLASH1
 
  //Erase
  CFLASH1.MCR.B.ERS = 1;
  CFLASH1.HSR.R = 0x00000004;
  *(unsigned int *)0x000C0000 = 0xFFFFFFFF;
  CFLASH1.MCR.B.EHV = 1;
  while ((CFLASH1.MCR.B.DONE == 0));
  CFLASH1.MCR.B.EHV = 0;
  CFLASH1.MCR.B.ERS = 0;

  //Program
  CFLASH1.MCR.B.PGM = 1;
  *(unsigned int *)0x000C0000 = 0x11112222;
  *(unsigned int *)(0x000C0000 + 0x4) = 0x33334444;
  CFLASH1.MCR.B.EHV = 1;
  while ((CFLASH1.MCR.B.DONE == 0));
  CFLASH1.MCR.B.EHV = 0;
  CFLASH1.MCR.B.PGM = 0;

Notice that we can write only one double word at a time.

Read-While-Write is supported between banks, so the code should be executed from RAM or from another bank.

Regards,

Lukas

0 Kudos
Reply