MPC5643L Boot without VDD_HV_ADR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5643L Boot without VDD_HV_ADR

1,266件の閲覧回数
jinjingyang
NXP Employee
NXP Employee

Dear Sir,

 

I tested on MPC5643L EVB and found that the MCU can boot without applying VDD_HV_ADR.

But it get stuck at the following code:

//ME_GS Wait for external osc to stabilize.

    while(ME.GS.B.S_XOSC==0)    {};

Even I applied 5V to VDD_HV_ADR at this moment, the software was still stuck here.

Then I reset the MCU and it can run normally and complete all clock initialization.

 

Can you help explain the above boot process? Why would I be stuck at the crystal initialization?

And customer's question is what's the max allowed delay between VDD_HV_ADR and other supplies for MCU to boot successfully at the very first time.

 

Regards,

Jason Yang

ラベル(1)
0 件の賞賛
返信
1 返信

1,193件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Jason,

I think that this note from datasheet explains everything:

pastedImage_1.png

Regards,

Lukas

0 件の賞賛
返信