MPC5566 clkout frequency during flashloading

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5566 clkout frequency during flashloading

1,319 次查看
franzstemmer
Contributor II

Hello, I have a question to the MPC5566.

What is the clkout frequency during flashing the internal flash via lauterbach debugger?

greetings

Franz

0 项奖励
回复
1 回复

1,277 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Franz,

first, clock frequency depends on your configuration:

pastedImage_1.png

For example, if  you use default configuration and if you have 8MHz crystal, then system clock is 12MHz (see default PLL settings).

Clocks configuration can be changed in *.cmm scripts if needed. So, you should check which scripts you use. If there's no additional PLL configuration, then default clocks are used.

Regards,

Lukas

0 项奖励
回复