MPC5566 clkout frequency during flashloading

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5566 clkout frequency during flashloading

1,343 Views
franzstemmer
Contributor II

Hello, I have a question to the MPC5566.

What is the clkout frequency during flashing the internal flash via lauterbach debugger?

greetings

Franz

0 Kudos
Reply
1 Reply

1,301 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Franz,

first, clock frequency depends on your configuration:

pastedImage_1.png

For example, if  you use default configuration and if you have 8MHz crystal, then system clock is 12MHz (see default PLL settings).

Clocks configuration can be changed in *.cmm scripts if needed. So, you should check which scripts you use. If there's no additional PLL configuration, then default clocks are used.

Regards,

Lukas

0 Kudos
Reply