MPC5554 with external bus interface problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5554 with external bus interface problem

3,909件の閲覧回数
liumaomao
Contributor I

hi,

     I am using MPC5554 Evaluation Board for testing External SRAM (two slices of IS61WV102416BLL chip )and configured address 0x20000000. For example, store 0x40000 data in the external memory and then read it out.Why is the value written different from the value read?

 

Thanking you,

Regards

0 件の賞賛
返信
3 返答(返信)

3,741件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi,

You don't need to write your own EBI initialization, it is already done in the CodeWarrior template.

pastedImage_21.png

0 件の賞賛
返信

3,738件の閲覧回数
liumaomao
Contributor I

Hi, David, I have modified MPC5554_HWInit.c file in your way,but it is still incorrect.I need your help .Thank you

0 件の賞賛
返信

3,738件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Could you specify "incorrect" behavior? Actually, are you using our EVB or your own prototype board? Used memory does not seem to be the same as we should have installed on the EVB.

pastedImage_337.png

I would like to test it myself, but I have the board at work, currently being on forced home office..

0 件の賞賛
返信