MPC5553MZP132 Power down sequence

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5553MZP132 Power down sequence

1,433 Views
Carl725
NXP Employee
NXP Employee

I am looking at the power down sequence paragraph 3.7.3 of the MPC5553 data sheet and I would like to request clarification, to understand the power down sequence requirement.

 

In our application VRC33 is hardwired to GND.

VDD =1.5V and VDDSYN =3.3V

 

When I remove 5 VDC which generates the 3.3V and the 1.5V I get an output glitch on 10 different pins which are expected to stay low during power down.

These pins are ADDR13, ADDR12, ADDR11, ADDR10, ADDR9, ADDR8, CS3, CS2, CS1 AND CS0.

 

When the unexpected low to high glitch occurs on these outputs the voltages are as follows:

 

VDD = 1.5V

VDDSYN =2.2V

5V = 3.3V

 

Should my VDDSYN be below 2.0V when we produce a RESET?

Labels (1)
0 Kudos
Reply
1 Reply

1,334 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

VRC33 is recommended to have connected to 3.3V to remove power sequence requirements. But if you have it connected to ground, then sections 3.7.2 and 3.7.3 take place.

Could I see your power down sequence?

I think following sentence answers your question:

"VDDSYN or the RESET power must decrease to less than 2.0 V before the VDD power increases to its operating range."

0 Kudos
Reply