Doubts and Problem in Mpc5606b

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Doubts and Problem in Mpc5606b

2,307件の閲覧回数
akhilmalik
Contributor II

hi

1. Which pin(s) in MpC5606b is 5 volt output for connection with any other device.

2. In EMIOS the SAOC mode is not running on counter bus A even i've set BSL to 00.

 

 

please reply asap.

Thanks

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,082件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

  1. All GPIO pins in case device is powered by 5V.
  2. see attached example tested on TRK-MPC5606B

BR, Petr

0 件の賞賛
返信

2,082件の閲覧回数
akhilmalik
Contributor II

hi

i'm asking about the pin which provide 5V and sufficient current to run any sensor.

i hope u getting my point.

thanks

0 件の賞賛
返信

2,082件の閲覧回数
akhilmalik
Contributor II

hi

please reply a little soon.

its urgent.

thanks

0 件の賞賛
返信