MMU initialization for MPC5777C

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MMU initialization for MPC5777C

4,404件の閲覧回数
vrushalitaklika
Contributor III

I am looking for MMU initilization for MPC5777C MCU. Can someone help with example or reference document for MMU programming in S32 IDE.

Regards

Vrushali

0 件の賞賛
返信
4 返答(返信)

2,938件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

There MMU is described in core reference manual:

http://cache.nxp.com/assets/documents/data/en/reference-manuals/e200z760RM.pdf?fsrch=1&sr=1&pageNum=... 

And here is the example of TLB configuration:

#*****************************
# configure the MMU
#*****************************
    e_lis   r3,0x1001
    mtspr   mas0,r3
    e_lis   r3,0xC000
    e_or2i  r3,0x0700
    mtspr   mas1,r3
    e_lis   r3,0x0000
    e_or2i  r3,0x0020
    mtspr   mas2,r3
    e_lis   r3,0x0000
    e_or2i  r3,0x003F
    mtspr   mas3,r3
    msync     # Synchronize in case running from flash
    tlbwe
    se_isync  # Synchronize in case running from flash

You could also check our example codes here:

https://community.nxp.com/docs/DOC-329623 

Peter

0 件の賞賛
返信

2,938件の閲覧回数
vrushalitaklika
Contributor III

Can we use the MMU initialisation given in startup.s file which is created when new project is created in studio s32

Here iscode from statup.s file

#ifdef __ghs__ /* GreenHills */
.section .startup, axv
.vle

.align 3 ;# 8 bytes

.extern main
.extern __SRAM_SIZE
.extern __SRAM_BASE_ADDR
.extern __DATA_SIZE
.extern __DATA_ROM_ADDR
.extern __DATA_SRAM_ADDR
.extern __SDATA_SIZE
.extern __SDATA_ROM_ADDR
.extern __SDATA_SRAM_ADDR
.extern __BSS_START
.extern __BSS_END
.extern __BSS_SIZE
.extern __SP_INIT
.extern _SDA_BASE_
.extern _SDA2_BASE_
#endif
#ifdef __GNUC__ /* GCC */
.section .startup, "ax"
#endif
#ifdef __DCC__ /* Diab */
.section ".startup",4,rx
#endif
.globl _start

_start:


;#****************************** Turn off SWTs ********************************
#if defined(DISABLE_SWTA)
;#SWT_A
e_lis r4, 0xFFF3
e_or2i r4, 0x8000

e_li r3, 0xC520
e_stw r3, 0x10(r4)

e_li r3, 0xD928
e_stw r3, 0x10(r4)

e_lis r3, 0xFF00
e_or2i r3, 0x010A
e_stw r3, 0(r4)
#endif
#if defined(MMU_CONFIG)
;#****************************** MMU configuration ********************************
e_lis r3, 0x1001
mtspr 624, r3

e_lis r4, 0xC000
e_or2i r4, 0x0480
mtspr 625, r4

e_lis r5, 0x4000
e_or2i r5, 0x0028
mtspr 626, r5

e_lis r6, 0x4000
e_or2i r6, 0x003f
mtspr 627, r6

tlbwe

e_lis r3, 0x1000
mtspr 624, r3

e_lis r4, 0xC000
e_or2i r4, 0x0700
mtspr 625, r4

e_lis r5, 0x0000
e_or2i r5, 0x0020
mtspr 626, r5

e_lis r6,0x0000
e_or2i r6, 0x003f
mtspr 627, r6

tlbwe

e_lis r3, 0x1002
mtspr 624, r3

e_lis r4, 0xC000
e_or2i r4, 0x0580
mtspr 625, r4

e_lis r5, 0xFFE0
e_or2i r5, 0x002A
mtspr 626, r5

e_lis r6, 0xFFE0
e_or2i r6, 0x003f
mtspr 627, r6

tlbwe

e_lis r3, 0x1003
mtspr 624, r3

e_lis r4, 0xC000
e_or2i r4, 0x0700
mtspr 625, r4

e_lis r5, 0x2000
e_or2i r5, 0x0020
mtspr 626, r5

e_lis r6,0x0000
e_or2i r6, 0x003f
mtspr 627, r6

tlbwe

e_lis r3, 0x1004
mtspr 624, r3

e_lis r4, 0xC000
e_or2i r4, 0x0580
mtspr 625, r4

e_lis r5, 0xC3E0
e_or2i r5, 0x002A
mtspr 626, r5

e_lis r6, 0xC3E0
e_or2i r6, 0x003f
mtspr 627, r6

tlbwe
#endif
;#*********************** Turn off Core Watchdog Timer*************************
e_li r3, 0x0000
mtspr 340, r3

;#********************************* Enable BTB ********************************
;# Flush & Enable BTB - Set BBFI bit in BUCSR
e_li r3, 0x201
mtspr 1013, r3
se_isync

;#**************************** Init Core Registers ****************************
;# The E200Z4 core needs its registers initialising before they are used
;# otherwise in Lock Step mode the two cores will contain different random data.
;# If this is stored to memory (e.g. stacked) it will cause a Lock Step error.

;# GPRs 0-31
e_li r0, 0
e_li r1, 0
e_li r2, 0
e_li r3, 0
e_li r4, 0
e_li r5, 0
e_li r6, 0
e_li r7, 0
e_li r8, 0
e_li r9, 0
e_li r10, 0
e_li r11, 0
e_li r12, 0
e_li r13, 0
e_li r14, 0
e_li r15, 0
e_li r16, 0
e_li r17, 0
e_li r18, 0
e_li r19, 0
e_li r20, 0
e_li r21, 0
e_li r22, 0
e_li r23, 0
e_li r24, 0
e_li r25, 0
e_li r26, 0
e_li r27, 0
e_li r28, 0
e_li r29, 0
e_li r30, 0
e_li r31, 0

;# Init any other CPU register which might be stacked (before being used).

mtspr 1, r1 ;#XER
mtcrf 0xFF, r1
mtspr CTR, r1
mtspr 272, r1 ;#SPRG0
mtspr 273, r1 ;#SPRG1
mtspr 274, r1 ;#SPRG2
mtspr 275, r1 ;#SPRG3
mtspr 58, r1 ;#CSRR0
mtspr 59, r1 ;#CSRR1
mtspr 570, r1 ;#MCSRR0
mtspr 571, r1 ;#MCSRR1
mtspr 61, r1 ;#DEAR
mtspr 63, r1 ;#IVPR
mtspr 256, r1 ;#USPRG0
mtspr 62, r1 ;#ESR
mtspr 8,r31 ;#LR

#ifdef START_FROM_FLASH
;#***************************** Initialise SRAM ECC ***************************/
;# Store number of 128Byte (32GPRs) segments in Counter
e_lis r5, __SRAM_SIZE@h # Initialize r5 to size of SRAM (Bytes)
e_or2i r5, __SRAM_SIZE@l
e_srwi r5, r5, 0x7 # Divide SRAM size by 128
mtctr r5 # Move to counter for use with "bdnz"

;# Base Address of the internal SRAM
e_lis r5, __SRAM_BASE_ADDR@h
e_or2i r5, __SRAM_BASE_ADDR@l

;# Fill SRAM with writes of 32GPRs
sram_loop:
e_stmw r0,0(r5) # Write all 32 registers to SRAM
e_addi r5,r5,128 # Increment the RAM pointer to next 128bytes
e_bdnz sram_loop # Loop for all of SRAM
#endif

;#*************** Load Initialised Data Values from Flash into RAM ************/
;# Initialised Data - ".data"
DATACOPY:
e_lis r9, __DATA_SIZE@ha # Load upper SRAM load size (# of bytes) into R9
e_or2i r9, __DATA_SIZE@l # Load lower SRAM load size into R9
e_cmp16i r9,0 # Compare to see if equal to 0
e_beq SDATACOPY # Exit cfg_ROMCPY if size is zero (no data to initialise)

mtctr r9 # Store no. of bytes to be moved in counter

e_lis r10, __DATA_ROM_ADDR@h # Load address of first SRAM load into R10
e_or2i r10, __DATA_ROM_ADDR@l # Load lower address of SRAM load into R10
e_subi r10,r10, 1 # Decrement address to prepare for ROMCPYLOOP

e_lis r5, __DATA_SRAM_ADDR@h # Load upper SRAM address into R5 (from linker file)
e_or2i r5, __DATA_SRAM_ADDR@l # Load lower SRAM address into R5 (from linker file)
e_subi r5, r5, 1 # Decrement address to prepare for ROMCPYLOOP

DATACPYLOOP:
e_lbzu r4, 1(r10) # Load data byte at R10 into R4,incrementing (update) ROM address
e_stbu r4, 1(r5) # Store R4 data byte into SRAM at R5 and update SRAM address
e_bdnz DATACPYLOOP # Branch if more bytes to load from ROM

;# Small Initialised Data - ".sdata"
SDATACOPY:
e_lis r9, __SDATA_SIZE@ha # Load upper SRAM load size (# of bytes) into R9
e_or2i r9, __SDATA_SIZE@l # Load lower SRAM load size into R9
e_cmp16i r9,0 # Compare to see if equal to 0
e_beq ROMCPYEND # Exit cfg_ROMCPY if size is zero (no data to initialise)

mtctr r9 # Store no. of bytes to be moved in counter

e_lis r10, __SDATA_ROM_ADDR@h # Load address of first SRAM load into R10
e_or2i r10, __SDATA_ROM_ADDR@l # Load lower address of SRAM load into R10
e_subi r10,r10, 1 # Decrement address to prepare for ROMCPYLOOP

e_lis r5, __SDATA_SRAM_ADDR@h # Load upper SRAM address into R5 (from linker file)
e_or2i r5, __SDATA_SRAM_ADDR@l # Load lower SRAM address into R5 (from linker file)
e_subi r5, r5, 1 # Decrement address to prepare for ROMCPYLOOP

SDATACPYLOOP:
e_lbzu r4, 1(r10) # Load data byte at R10 into R4,incrementing (update) ROM address
e_stbu r4, 1(r5) # Store R4 data byte into SRAM at R5 and update SRAM address
e_bdnz SDATACPYLOOP # Branch if more bytes to load from ROM


ROMCPYEND:

;#*************************** Enable ME Bit in MSR *****************************
mfmsr r6
e_or2i r6,0x1000
mtmsr r6

;#*************************** Enable SPE Bit in MSR *****************************
mfmsr r3
e_or2is r3,0x0200
mtmsr r3

;#****************** Invalidate and Enable the Instruction cache **************
__icache_cfg:
e_li r5, 0x2
mtspr 1011,r5

e_li r7, 0x4
e_li r8, 0x2
;#e_lwi r11, 0xFFFFFFFB
e_lis r11,0xFFFF
e_or2i r11,0xFFFB

__icache_inv:
mfspr r9, 1011
and. r10, r7, r9
e_beq __icache_no_abort
and. r10, r11, r9
mtspr 1011, r10
e_b __icache_cfg

__icache_no_abort:
and. r10, r8, r9
e_bne __icache_inv

mfspr r5, 1011
e_ori r5, r5, 0x0001
se_isync
;#msync
mtspr 1011, r5

;#****************** Invalidate and Enable the Data cache **************
__dcache_cfg:
e_li r5, 0x2
mtspr 1010,r5

e_li r7, 0x4
e_li r8, 0x2
e_lis r11,0xFFFF
e_or2i r11,0xFFFB

__dcache_inv:
mfspr r9, 1010
and. r10, r7, r9
e_beq __dcache_no_abort
and. r10, r11, r9
mtspr 1010, r10
e_b __dcache_cfg

__dcache_no_abort:
and. r10, r8, r9
e_bne __dcache_inv

mfspr r5, 1010
e_ori r5, r5, 0x0001
se_isync
msync
mtspr 1010, r5

;#****************************** Initialize BSS section ******************************/
bss_Init:
e_lis r9, __BSS_SIZE@h # Load upper BSS load size (# of bytes) into R9
e_or2i r9, __BSS_SIZE@l # Load lower BSS load size into R9 and compare to zero
e_cmp16i r9,0
e_beq bss_Init_end # Exit if size is zero (no data to initialise)

mtctr r9 # Store no. of bytes to be moved in counter

e_lis r5, __BSS_START@h # Load upper BSS address into R5 (from linker file)
e_or2i r5, __BSS_START@l # Load lower BSS address into R5 (from linker file)
e_subi r5, r5, 1 # Decrement address to prepare for bss_Init_loop

e_lis r4, 0x0

bss_Init_loop:
e_stbu r4, 1(r5) # Store zero byte into BSS at R5 and update BSS address
e_bdnz bss_Init_loop # Branch if more bytes to load

bss_Init_end:

;#****************************** Configure Stack ******************************/
e_lis r1, __SP_INIT@h ;# Initialize stack pointer r1 to
e_or2i r1, __SP_INIT@l ;# value in linker command file.

e_lis r13, _SDA_BASE_@h ;# Initialize r13 to sdata base
e_or2i r13, _SDA_BASE_@l ;# (provided by linker).

e_lis r2, _SDA2_BASE_@h ;# Initialize r2 to sdata2 base
e_or2i r2, _SDA2_BASE_@l ;# (provided by linker).

e_stwu r0,-64(r1) ;# Terminate stack.

#if defined(HW_INIT)
;# perform hardware init prior to main
e_bl hw_init
#endif
;# Jump to Main
e_bl main

0 件の賞賛
返信

2,938件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Nice spam. Why do you not used attach file?

In general you can use whatever you want. If you will use MMU init from startup file of S32DS I see no issue here.

If you need to initialize MMU in some "not general" way, then it is up to you to do modifications.

Peter

0 件の賞賛
返信

2,938件の閲覧回数
vrushalitaklika
Contributor III

Thanks Petere. Sorry attachement option was not available and hence I had to copy paste everything here.

your reply helps..

0 件の賞賛
返信