MC33907 IO_45 error detection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC33907 IO_45 error detection

ソリューションへジャンプ
2,124件の閲覧回数
chshli
Contributor II

Hi ,

     According to MC33907 UM,IO_45 error detection can lead to FS0B low.

     But what are the conditions of IO_45 error detection? And how to assert FS0B low by IO_4 fault inject?

Thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
2,008件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

The error will be detected when IO_4=0 for >20us and IO_5=1 (no acknowledgement). In that case, FS0B is asserted low after 9.7ms (T_ACK_FS). To enable this, the IO_45_FS bit in the INIT_FSSM1 needs to be set to 1 ( = safety critical).

Please let me know if there are any other questions.

Regards,

Tomas

PS: If this answer helps to solve your question, please mark it as "Correct". Thank you.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,009件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

The error will be detected when IO_4=0 for >20us and IO_5=1 (no acknowledgement). In that case, FS0B is asserted low after 9.7ms (T_ACK_FS). To enable this, the IO_45_FS bit in the INIT_FSSM1 needs to be set to 1 ( = safety critical).

Please let me know if there are any other questions.

Regards,

Tomas

PS: If this answer helps to solve your question, please mark it as "Correct". Thank you.

0 件の賞賛
返信