Loopback modes with TJA1100 Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Loopback modes with TJA1100 Issue

3,995 Views
ahmedsaber
Contributor I

Hello All,

In an Automotive project we are using TJA1100 as a PHY, I'm trying to validate the functionality of the 100BASE-T1 PCS and PMA functions.

So according to the TJA1100's datasheet in the loopback section,

pastedImage_1.png

I followed the steps to put the PHY in the external loopback mode as mentioned in the application notes AN12088

 pastedImage_2.png

But when I put the PHY in the external loopback I sent the data successfully but I didn't receive anything

To validate the loopback at all I tried the internal loopback mode, it works fine as Tx and Rx but also there was an issue which is the data transmitted on the bus, while it must not

Any answer please

Thanks

Ahmed Saber

Labels (1)
0 Kudos
Reply
4 Replies

3,552 Views
thosewhowish2b
Contributor II

Hello Ahmed,

did you have any luck on this?

By the way, how did you manage to do even the internal loopback? So far I have had no success with that.

Best regards.

0 Kudos
Reply

3,907 Views
misonyo
Contributor I

hello ,can you tell me what's the problem you meet? how to solve this problem??

i meet the same problem like you.

0 Kudos
Reply

3,910 Views
Bulat
NXP Employee
NXP Employee

Can you describe how you run external loopback test step by step?
What is TRX pins connection during the test?

Regards,

Bulat

0 Kudos
Reply

3,900 Views
misonyo
Contributor I
Spoiler
 

hello,should I connect TRX PINS to other PHYs?  I meet the same problem when i use TJA1101.

0 Kudos
Reply