Lifetime timer on MPC5777C

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Lifetime timer on MPC5777C

ソリューションへジャンプ
2,236件の閲覧回数
20Sidar04
Contributor III

Dear Mr/Mrs,

I am working on lifetime timer on MPC5777C. I set my contiunging period maximum.

When I try to debug my controller on S32, My current_uptime variable is like below;

Start: 1111 1111 1111 1111 1111 1111 1111 1111 | 0000 0000 0000 0000 0000 0000 0000 0000

Time N = 1111 1111 1111 1111 1111 1111 1111 0110 | 0000 0000 0000 0000 0000 0000 0000 0000
Time N-1 = 1111 1111 1111 1111 1111 1111 1111 0101 | 0000 0000 0000 0000 0000 0000 0000 0000
Time N-2 = 1111 1111 1111 1111 1111 1111 1111 0100 | 0000 0000 0000 0000 0000 0000 0000 0000
Time N-3 = 1111 1111 1111 1111 1111 1111 1111 0011 | 0000 0000 0000 0000 0000 0000 0000 0000
Time N-4 = 1111 1111 1111 1111 1111 1111 1111 0010 | 0000 0000 0000 0000 0000 0000 0000 0000

But it should be FFFFFFFFF start of system. What make could it like that?

 

I share my source code below;

void lifetime_timer_init(void)
{
PIT->MCR |= 4; // clock for RTI Timers is enabled
PIT->TIMER[1].LDVAL = 0x0xFFFFFFFF; // setup timer 1 for maximum counting period
PIT->TIMER[1].TCTRL |= 5; // chain timer 1 to timer 0, timer1 start, disable timer1 interrupt
PIT->TIMER[0].LDVAL= 0xFFFFFFFF; // setup timer 0 for maximum counting period
PIT->TIMER[0].TCTRL |= 1; // start timer 0
}

lifetime_timer_init();

while(1)
{

current_uptime = 0;
current_uptime = (PIT->LTMR64H );
current_uptime= current_uptime <<32;
current_uptime = current_uptime + PIT->LTMR64L;

}

 

Best Regards,

タグ(3)
0 件の賞賛
返信
1 解決策
2,207件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

I checked your code and it works fine. Below what I saw in S32DS

PetrS_0-1631688990985.png

BR, Petr

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,208件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

I checked your code and it works fine. Below what I saw in S32DS

PetrS_0-1631688990985.png

BR, Petr

 

0 件の賞賛
返信