LBIST 4 and 3 failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LBIST 4 and 3 failed

Jump to solution
1,836 Views
ORaissouni
Contributor III

Hi folks,

We had the Online LBISTs always running successful until we had to change PER_CLK configuration from 150 to 100 MHz, then, LBIST 3 and LBIST 4 both fail.
Is there any explanation why LBIST 3 and LBIST 4 fail with PER_CLK equal to 100MHz ?

With best Regards

Omar

0 Kudos
Reply
1 Solution
1,798 Views
ORaissouni
Contributor III

Hello,

The adjustment of the STC WDG did not fix the issue; extending the STUC WDG timer to the max (0xFFFFFFFF) did not work.
However, the issue was fixed by setting the clock source of PER_CLK to CORE_CLK.

Thank you for you support.

View solution in original post

0 Kudos
Reply
2 Replies
1,799 Views
ORaissouni
Contributor III

Hello,

The adjustment of the STC WDG did not fix the issue; extending the STUC WDG timer to the max (0xFFFFFFFF) did not work.
However, the issue was fixed by setting the clock source of PER_CLK to CORE_CLK.

Thank you for you support.

0 Kudos
Reply
1,820 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I expect the slower execution will also require STCU watchdog to be adjusted accordingly.

Please always use the validated test scenarios by NXP.

Best regards,

Peter

0 Kudos
Reply