Issue with PLL Lock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,426件の閲覧回数
bjrajendra
Senior Contributor I

Hello all,

I'm using MPC5602P device.

I wrote the code so as to initialize the clock with PLL. The code stuck as shown in the below screenshot.

pastedImage_1.png

Kindly help in this regard,

Raju

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
2,310件の閲覧回数
bjrajendra
Senior Contributor I

Hi David,

Thanks for your response.

I used one of the example projects to develop the code and it has been working normally all the time.

I solved the issue it is actually the debugger cable connecting to the board is loose.

Once again Thanks for the support,

Raju

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,310件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, here you may find a example code showing also PLL setting:

Example MPC5604P PinToggleStationery CW210 

Also I may recommended following excel tool:

https://community.nxp.com/docs/DOC-332694 

2,311件の閲覧回数
bjrajendra
Senior Contributor I

Hi David,

Thanks for your response.

I used one of the example projects to develop the code and it has been working normally all the time.

I solved the issue it is actually the debugger cable connecting to the board is loose.

Once again Thanks for the support,

Raju

0 件の賞賛
返信