IBIS model for MPC5534 Microcontroller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IBIS model for MPC5534 Microcontroller

6,742件の閲覧回数
nileshkhupase
Contributor I

Dear sir or Madam,

 

Is there an IBIS model for MPC5534 Microcontroller?

 

Many Thanks in advance.

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

5,346件の閲覧回数
Shweta_chendake
Contributor I

 can we use IBIS model of MPC5554 instead of MPC5534?

and if yes then please send the  associated pin numbers in the MPC5554 model that have the same function as those in the MPC5534 model.

  • SCKC( K20)-
  • SINC( J20) -
  • SOUTC (K22) -
  • PCSC3 (AB18) -
  • SCKD (M21) -
  • SIND (K19) -
  • SOUTD (N19)-
  • PCSD0 (J22) -

 

Ans if No, can you please send the generic IBIS model for MPC5534?

0 件の賞賛
返信

6,607件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Unfortunately we don't have a specific ibis model for the MPC5534.

We have a general ibis model for the MPC555x/MPC556x family of products, on the link below:

http://www.nxp.com/webapp/sps/download/license.jsp?colCode=MPC5554_IBIS&location=null&Parent_nodeId=...

The name of the file states MPC5554, however, it applies to all MPC555x/MPC556x family devices.

0 件の賞賛
返信

6,606件の閲覧回数
nileshkhupase
Contributor I

Dear Sir or Madam,

Thank you very much for your reply. Can I refer the same IBIS model for MPC5534 device? Does MPC5534 belong to MPC555x/MPC556x family?

Best regards,

Nilesh Khupase

0 件の賞賛
返信

6,606件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

To be more precise it is MPC5500 family and devices are somehow compatible to each other:

http://cache.nxp.com/files/32bit/doc/eng_bulletin/EB659.pdf

0 件の賞賛
返信

6,605件の閲覧回数
nileshkhupase
Contributor I

Hi David,

That means we do not have IBIS model for MPC5500 family. Can we use the available IBIS model (MPC5554)?

Thanks,

Nilesh

0 件の賞賛
返信