I am unable to write and read more than 10 characters in to EEPROM demo program for the MPC5748G

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I am unable to write and read more than 10 characters in to EEPROM demo program for the MPC5748G

Jump to solution
2,446 Views
priya_p
Contributor IV

I am using MPC5748G dev kit and I tried running EEPROM emulator "demo" program in the S32DS for power architecture. I changed the size to 40. But when ever I am trying to write to the EEPROM more than 10 characters it is only writing up to 10 characters. I tried reading it back, but in the buffer I can only see 10 characters. Please help me in this regard.

 

I am attaching demo code along with this mail.

0 Kudos
Reply
1 Solution
2,435 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I did quick test on my side and it works as expected. I just changed the size like this:

lukaszadrapa_0-1624891489824.png

And that's the only change I did in the project.

Then I confirmed first record is programmed as expected:

lukaszadrapa_1-1624891583081.png

Second one is also OK:

lukaszadrapa_2-1624891630165.png

This is state of cleared buffer after programming of all records and before reading of a record with id 10:

lukaszadrapa_3-1624891699846.png

And finally, I can see that the record is read as expected:

lukaszadrapa_4-1624891741113.png

 

So, I can see no problem here.

Regards,

Lukas

View solution in original post

4 Replies
2,347 Views
priya_p
Contributor IV

I am using MPC5748G dev kit and i am executing it on S32DS. I have a query regarding EEPROM. how to select our desired address space in EEPROM and what is the relation between id and EEPROM?

0 Kudos
Reply
2,381 Views
priya_p
Contributor IV

Thank You so much.. It worked. But I have a query regarding this EEPROM demo code. suppose I need to write data into EEPROM in every 1 minute. I can use PIT Timer for that but, how to write into EEPROM without losing previous data ? I need to take value and put into EEPROM continuously. For the first it write perfectly. But for the 2nd loop it is going to Devassert and stuck in infinite loop. So, how to write in to a EEPROM in a loop?

0 Kudos
Reply
2,436 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I did quick test on my side and it works as expected. I just changed the size like this:

lukaszadrapa_0-1624891489824.png

And that's the only change I did in the project.

Then I confirmed first record is programmed as expected:

lukaszadrapa_1-1624891583081.png

Second one is also OK:

lukaszadrapa_2-1624891630165.png

This is state of cleared buffer after programming of all records and before reading of a record with id 10:

lukaszadrapa_3-1624891699846.png

And finally, I can see that the record is read as expected:

lukaszadrapa_4-1624891741113.png

 

So, I can see no problem here.

Regards,

Lukas

2,380 Views
priya_p
Contributor IV

hank You so much.. It worked. But I have a query regarding this EEPROM demo code. suppose I need to write data into EEPROM in every 1 minute. I can use PIT Timer for that but, how to write into EEPROM without losing previous data ? I need to take value and put into EEPROM continuously. For the first it write perfectly. But for the 2nd loop it is going to Devassert and stuck in infinite loop. So, how to write in to a EEPROM in a loop?

0 Kudos
Reply