How to use PLL clock as monitoring clock in CMU_PLL(CMU_0)-MPC5746R

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use PLL clock as monitoring clock in CMU_PLL(CMU_0)-MPC5746R

Jump to solution
3,339 Views
renjithr
Contributor I

Hi,

I want to use CMU for PLL fault check in MPC5746R

Is it possible to use PLL clock as a monitoring clock in CMU_0 (CMU_PLL)..?

- If Yes, any specific configuration is required to select the monitored clock source as PLL.

Please find the attachment ,which is captured from MPC5746RRM.pdf

Thanks ,

Renjith

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
3,133 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi Renjith,

The PLL0_PHI clock output is connected to the CLKMN1 input clock of the MPC5746R’s CMU_0 module.

This clock can only be monitored, cannot be monitoring/referencing clock. The CLKMN1 (PLL0) is compared to high-limit and low-limit frequencies to determine wheter the CLKMN1 frequency is between the specified limits.

These limits are set by the CMU_0.HFREFR and CMU_0.LFREFR registers as

 

high-limit freq = (HFREF ÷ 16) × (fCLKMT0_RMN ÷ 4)

low-limit freq = (LFREF ÷ 16) × (fCLKMT0_RMN ÷ 4).

 

The fCLKMT0_RMN is equal to IRC_OSC clock

BR, Petr

View solution in original post

0 Kudos
Reply
1 Reply
3,134 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi Renjith,

The PLL0_PHI clock output is connected to the CLKMN1 input clock of the MPC5746R’s CMU_0 module.

This clock can only be monitored, cannot be monitoring/referencing clock. The CLKMN1 (PLL0) is compared to high-limit and low-limit frequencies to determine wheter the CLKMN1 frequency is between the specified limits.

These limits are set by the CMU_0.HFREFR and CMU_0.LFREFR registers as

 

high-limit freq = (HFREF ÷ 16) × (fCLKMT0_RMN ÷ 4)

low-limit freq = (LFREF ÷ 16) × (fCLKMT0_RMN ÷ 4).

 

The fCLKMT0_RMN is equal to IRC_OSC clock

BR, Petr

0 Kudos
Reply