Hi Renjith,
The PLL0_PHI clock output is connected to the CLKMN1 input clock of the MPC5746R’s CMU_0 module.
This clock can only be monitored, cannot be monitoring/referencing clock. The CLKMN1 (PLL0) is compared to high-limit and low-limit frequencies to determine wheter the CLKMN1 frequency is between the specified limits.
These limits are set by the CMU_0.HFREFR and CMU_0.LFREFR registers as
high-limit freq = (HFREF ÷ 16) × (fCLKMT0_RMN ÷ 4)
low-limit freq = (LFREF ÷ 16) × (fCLKMT0_RMN ÷ 4).
The fCLKMT0_RMN is equal to IRC_OSC clock
BR, Petr