How to use General purpose registers in C code with MPC574x?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to use General purpose registers in C code with MPC574x?

1,945 次查看
kshitij_dadheka
Contributor II

I am trying to port the MC33771 library which was written for S32K144(ARM architecture) to a MPC574x(Power architecture) controller. A piece of MC33771's sample code in bcc_wait.c is writtten in assembly where it waits for cycles in multiples of 4.

 pastedImage_1.png

From the Power architecture instruction set I understand that "movs" needs to be changed to "mr" or some other equivalent instruction and "r0" can be a general-purpose register like GPR0 to GPR31.

But when I try to use GPR0-31 it throws a relocation error

pastedImage_2.png

martinkovarTomasVaverka

Questions:

1. What is the correct syntax to use the GPR registers inline with C-code?

2. What are other ways to count cycles in MPC574x? 

Thanks in advance

标签 (1)
0 项奖励
回复
2 回复数

1,800 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

first important point: due to pipelining, flash wait states, cache, other bus masters and priorities on crossabar etc., it's not easy to generate exact delays using asm or C code. This was easy on older and simpler devices where the timing of everything was strictly given. But features which increase the performance insert relatively high variability when talking about timing.

So, my usual recommendation is: if the timing is not critical and you can accept relatively high inaccuracy, use just simple delay loops like:

for(i=0; i<delay; i++)

   __asm("nop");

... or whatever like this. I can't see a benefit to write this in asm.

If the timing is critical, use a timer like PIT or STM to generate accurate delays.

Example MPC5744P STM timer S32DS Power 2017.R1 

Example MPC5744P PIT triggering interrupts GHS614 

And to asnwer your original question, here is an example of inline asm syntax (writing value 0xA1000F00 to SPR register 624 using r3 register):

    __asm("e_lis %r3, 0xA100");
    __asm("e_or2i %r3, 0x0F00");
    __asm("mtspr 624, %r3");

Regards,

Lukas

0 项奖励
回复

1,800 次查看
kshitij_dadheka
Contributor II

Thank you lukaszadrapa‌. That was really helpful

0 项奖励
回复